Locate in OPC Data Explorer

This option is only available if:

Select the Locate in OPC Data Explorer option for Geo SCADA Expert to display the OPC Data Bar and highlight the item in the hierarchical ‘tree’ structure within that Explorer Bar.

Also see Locate in Database Explorer.

You can also locate an item in the OPC Data Bar by using the Locate command on the ViewX ribbon (see Display an Explorer Bar).


Disclaimer

Geo SCADA Expert 2021