Remove Alarms

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Remove Alarms

WARNING

LACK OF ALARM NOTIFICATION

Use the Remove Alarms option with care. Before using the option, we strongly recommend that you perform a risk analysis to ensure that the removal of existing alarms will not pose a danger to people or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Use the Remove Alarms option on the Object Menu to remove any acknowledged alarms on the selected item.

Select the option on a point to remove the acknowledged alarms on that point.

Select the option on a Group or Group Instance to remove the acknowledged alarms on the items in that Group or Group Instance (and in any subgroups within that Group or Group Instance).

For more information, see Remove an Alarm.

If using this pick action with the Automation Interface, you need to specify the method name RemoveAlarm.


Disclaimer

Geo SCADA Expert 2021