Rename a Document in your Operator Document Store

You can rename any of the documents that are stored in your Operator Document Store(s). This is useful when a document has been provided with a misleading name or there is a mistake in the name.

To rename a document in your Operator Document Store:

  1. Log on to ViewX.
  2. Display your Operator Document Stores (see Access Your Operator Document Stores).
  3. Expand your Operator Document Stores until you locate the document that you want to rename.
  4. Right-click on the document, then select the Rename option from the context sensitive menu.
    The document is selected automatically, ready for you to define its name.
  5. Overwrite or amend the existing name as required, then press the Enter key or select another part of the interface to confirm your entry.

Disclaimer

Geo SCADA Expert 2021