ViewX Client Session Expiry due to User Inactivity

Geo SCADA Expert supports the ability to hide displays from view should no activity be detected for a period of time on a ViewX client. The feature is a security measure, in case a user has forgotten to log off and has left their workstation unattended. If the feature is enabled on your user account, an administrator will have specified the amount of time that can elapse before the feature is triggered (the Inactivity Logout time). If no activity has been detected for longer than this amount of time on the ViewX client onto which you are logged, the Geo SCADA Expert displays that are open on that ViewX client will be hidden from view and a dialog box will be displayed.

If you are working with a Multi-Monitor Setup when the user session expires, Geo SCADA Expert displays will be hidden from view on each of the monitors that the ViewX client is configured to use.

Select the OK button to continue.
A further dialog box is displayed.

Perform one of the following:

NOTICE

POTENTIAL SECURITY BREACH

We strongly recommend that you close any ViewX displays that are open before you log off ViewX. If any displays are left open, they will be visible to the next user to access that particular ViewX client (providing that their user account enables them to access those particular displays).
Failure to follow these instructions can result in sensitive data or unsaved updates being left on display for other users to access.

Disclaimer

Geo SCADA Expert 2021