Associated with: All items
This status attribute comprises a standard description of the type of item.
Use the attribute in conjunction with the Full Name status attribute and, if applicable, the Source status attribute, to ascertain a particular item’s function and location on your system.
Example:
          Modbus Digital Point
  (Indicating that the item is the type of digital point that is supported by Geo SCADA Expert's Modbus driver. (The point represents digital data on a device with which Geo SCADA Expert communicates using the Modbus protocol, via Geo SCADA Expert's Modbus driver.))