Use Copy and Paste in Virtual ViewX

When using Virtual ViewX, be aware that you cannot use Copy and Paste buttons or menu options in Geo SCADA Expert to copy content from Virtual ViewX into another application. This is a browser security feature. To copy content from Virtual ViewX into another application, such as Notepad, you have to use the keyboard shortcuts or the menu options provided by the web browser. The keyboard shortcuts that you can use include:

Keys Action
CTRL + A Selects all of the content in the active field
CTRL + C Copies the selected content to the local machine's clipboard
CTRL + V Pastes the copied content from the clipboard

Further Information

Copy and paste status attribute content: see Use the Status Display Buttons.


Disclaimer

Geo SCADA Expert 2021