Alarm Limits for WITS Counter-Type Points

You need to set the alarm limits for each WITS counter-type point so that when the value of the point rises above the normal range of values, Geo SCADA Expert raises a suitable alarm or logs an event.

WITS counter-type points can have up to five alarm limits that you can configure to suit your requirements. The Device Profile defines how many alarm limits a Field Device supports (see Display a WITS Device Profile).

Use the fields within the Alarm Limits section of the <Point Type> tab to specify the alarm limit properties.

The upper part of the Alarm Limits section has a row of fields for each alarm limit. The number of rows you can use is defined by the Device Profile for your field device. The point Form shows the maximum number of available rows.

WITS specifies that the list of alarm limits is hierarchical, so the highest limit number has to have the highest limit value. For example, limit 5 has to have a higher limit value than limit 4, limit 4 has to have a higher limit value than limit 3 and so on. You also have to use the limits consecutively. For example, if your field device supports 3 limits, you use limits 1, 2 and 3.

The Normal state defines the usual operating range for the plant.

The following Alarm Limits properties are WITS specific:

The other Alarm Limits fields are common to many drivers (see Configure the Limits for a Counter-Type Point and see Define Whether a Counter-Type Point's Limits can be Tuned).

NOTE: The availability of some of these properties is dependent on your field device supporting that feature. For more details, see WITS Device Profiles.


Disclaimer

Geo SCADA Expert 2021