Configuration Reports for WITS Field Devices

If Geo SCADA Expert is unable to import or upload configuration for a WITS Field Device, a configuration report is created. The configuration report details the invalid configuration that caused the import or upload to fail, so that you can locate and correct the errors.

To display the configuration report for a WITS Field Device, use the Display Config Report action (which requires the Configure permission). This action is available from the context-sensitive menu for WITS Outstation items, but only if a configuration import or upload attempt has failed.

When you select the Display Config Report action, Geo SCADA Expert either:

Or:

When the configuration report is displayed, you can see details of the invalid configuration. The information is provided in a tabular format, and you can use it to locate the incorrect configuration.

Display Config Report - Example of Report

There are up to 4 sections to the report (sections are omitted if they are not applicable):

 

Further Information

Display Config Report pick action

Import Configuration

Upload Configuration (WITS Outstation)


Disclaimer

Geo SCADA Expert 2021