Download Configuration (WITS Outstation)

Associated with: WITS Outstations.

Security permission required to access this pick action: Configure.

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Downloading configuration from Geo SCADA Expert to a WITS Field Device can cause the Field Device to reset (a reset occurs if the bulk configuration file is downloaded). The Device Profile defines whether a Field Device will perform a DNP3 cold reset or only a warm reset. For this reason, always ensure that it is safe to allow the outstation to reset before issuing an All Configuration or Changed Configuration Only download.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE

INOPERABLE DEVICE

Always verify that the outstation’s communications settings are configured correctly in Geo SCADA Expert before triggering a Download Configuration action. Should the configuration conflict with the actual setup at the outstation, normal communications between Geo SCADA Expert and the outstation may cease. For example, communications could be lost if there is a mismatch between the downloaded port configuration and the actual ports that the outstation is using.

Only attempt to download configuration when there is sufficient time to recover the situation (should a configuration mismatch occur).

Failure to follow these instructions can result in inoperable equipment.

If your Field Device supports configuration download, you can use the Download Configuration action to download a Field Device's configuration from Geo SCADA Expert. You can find out if your Field Device supports configuration download by looking at its Device Profile (see WITS Device Profiles).

Being able to download the configuration from Geo SCADA Expert means that you can configure your Field Device remotely (using Geo SCADA Expert and/or a vendor supplied configuration tool). For more information, see WITS Configuration Strategies.

When you select Download Configuration, a Download Configuration window is displayed. It prompts you to select the type of configuration download that Geo SCADA Expert is to perform.

Download Configuration - WITS Outstation

Choose from:

With PSTN and ‘On Demand’ outstations, the Download Configuration window may also have a Queue check box.

For details on the Queue setting, which (see Queue Check Box).

When downloading configuration, any new Application Programs created in the Geo SCADA Expert database will also be created in the Field Device. Any Applications Programs that have been deleted from the Geo SCADA Expert database, or taken out of service, will be deleted from the Field Device. Any existing Application Programs in the Geo SCADA Expert database are updated in the Field Device with the new program file (if the version of the program file is different or if you select the All Configuration option).


Disclaimer

Geo SCADA Expert 2021