Exporting a WITS Device Profile XML File

You can use ViewX's Export Profile action to export a copy of a device profile XML file to another location, for example, to a network drive. This means you can use Geo SCADA Expert as a repository for your Field Device profiles: you can import the vendor-supplied XML file, store and view it in Geo SCADA Expert, and export it if required. The XML file that Geo SCADA Expert exports is exactly the same as the file that was originally supplied by the vendor.

To export a WITS device profile XML file from Geo SCADA Expert:

  1. Run ViewX and log on via a user account that has the Configure permission.
  2. Display the Database Bar (see Display an Explorer Bar).
  3. Use the Database Bar to browse to the Device Profile database item that contains the XML file you want to export.
  4. Right-click on the Device Profile item and select the Export Profile option.
    The Export Profile window is displayed.

    The Export Profile option is only available if the Device Profile contains an XML file (i.e. a device profile has been imported into the item previously).

  5. Use the Export Profile window to select the required location for the export file and also to give the file a name. We recommend that you define a descriptive name so that other users can easily identify the purpose of the XML file.
  6. Select the Save button.

Further Information

WITS Device Profiles

Configuring a WITS Device Profile

Importing a WITS Device Profile XML File

Display a WITS Device Profile


Disclaimer

Geo SCADA Expert 2021