Historic Data Filter for WITS Database Points

You can use the WITS Point Form to specify what type of data is stored in the Geo SCADA Expert historic database for a point. The Historic Data Filter settings allow you to choose from:

You can only specify the Historic Data Filter settings for points that have Historic enabled (see Defining Historic Details for a Point).

Many people find that the default settings (for points with Historic enabled) are suitable for their needs. The default settings have State Change Events, Other Events and Periodic enabled.

To specify which point data is stored historically:

  1. Log on to ViewX via a user account that has the Configure permission, and then display the Form for the WITS database point (see Display a Form).
  2. Select the <Point Type> tab, for example, select the Analog Point tab on the Analog Point Form.
  3. In the Historic Data Filter section, use the check boxes to specify whether the Geo SCADA Expert stores each type of data historically. (Select the appropriate check box to store the data historically; clear if you do not want to store the data historically).
  4. Save the configuration.

Further Information

Historic settings: see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration


Disclaimer

Geo SCADA Expert 2021