Host Address for WITS Network Connections

You can use the WITS Outstation Form to configure network connections between Geo SCADA Expert and a WITS Field Device. For each connection, you need to specify the host address of the Field Device (outbound) or Geo SCADA Expert server (inbound).

The settings at the top of the Form are for the outbound connection (Geo SCADA Expert to Field Device), and include a Host Address. In this Host Address field, you need to specify the IP address or domain name of the Field Device. There are two Host Address fields for Dual Networks: one for each network.

Host Address - Outbound Network Connection

Further down the Form, there is a Host Address field for each Inbound Connection. For the inbound connections, you need to specify the IP address or domain name of a Geo SCADA Expert server.

Host Address - Inbound Network Connections

If the Geo SCADA Expert server or WITS Field Device are behind a router, you may need to specify the IP address or domain name of the router. The router will then need to be configured to forward the connection to the Field Device/Geo SCADA Expert server.

Further Information

Configure a WITS Field Device to Initiate Only

Configure a WITS Field Device to Listen Only

Configure a WITS Field Device to Listen and Initiate via the Same Connection

Configure a WITS Field Device to Listen and Initiate via Separate Connections.


Disclaimer

Geo SCADA Expert 2021