Sequential Persistence

Sequential Persistence is when the separate Persistence durations of an analog point are configured so that:

Sequential Persistence only applies to analog points used by Field Devices that support a separate persistence for each limit.

Example:

Low 1, Persistence: 2S

Low 2, Persistence: 4S

Low 3, Persistence: 6S

Low 4, Persistence: 8S

This means that the Persistence Durations will expire in sequence, i.e. in Alarm Limit order. For example, if a point's value crosses Low 1 and Low 2 at the same time, the Persistence Duration for Low 1 will expire before the Persistence Duration for Low 2.

Further Information

Non-Sequential Persistence

Single Persistence Per Point

Separate Persistence Per Point Limit/State


Disclaimer

Geo SCADA Expert 2021