Trend Settings for WITS Minimum Points

You can display the trend, or movement, of the value of a WITS Minimum Point in the form of a graph.

The WITS Minimum Point is a type of analog point. Therefore, many of the fields in the Trend section of the Minimum tab are the same as those for other WITS analog points. The Maximum, Minimum andLogarithmic field values are inherited from the parent point (see Define an Analog Point's Trend Settings).


Disclaimer

Geo SCADA Expert 2021