Using a Configuration Application to Change Field Device Configuration

WITS Field Device manufacturers provide Configuration Applications that you can use to change the configuration of your Field Device(s). When you make configuration changes using a Configuration Application, the altered configuration has to be:

When you use a Configuration Application to edit the bulk configuration file for a Field Device, you need to allocate a new version. The new version has to be included in the filename when saving the bulk configuration file.


Disclaimer

Geo SCADA Expert 2021