Vendor Health Check Statuses

Associated with: WITS Outstations.

 

WITS Field Devices can send health check status information to Geo SCADA Expert for up to 32 vendor-specified attributes.

The Status display shows this health check status information on a separate line for each attribute. For each line, there is an attribute description followed by the attribute status. The status will be either True or False (to represent whether the attribute is set or clear).

You can find definitions of the vendor-specified health check attributes in the device profile ((see Display a WITS Device Profile)).


Disclaimer

Geo SCADA Expert 2021