Incremental Configuration File - Content and Syntax

In this topic, we describe the content of the incremental configuration files used by WITS Field Devices. The WITS-DNP3 standard does not specify a syntax for incremental configuration file names.

When saving or exporting incremental configuration files, we recommend that you give each incremental file the same name as its matching bulk configuration file, but use a different extension.

Incremental Configuration File

The incremental configuration file contains a series of records that define the following settings:

Other vendor-specific configuration settings are stored in the bulk configuration file.

Further Information

Bulk Configuration File - Content and Syntax.

Bulk Configuration and Incremental Configuration Files - Generation and Transfer.

WITS Configuration Strategies.


Disclaimer

Geo SCADA Expert 2021