User Account Created Automatically on the Virtual ViewX Server Machine
A user account is created automatically in Windows on the Virtual ViewX server machine when you install Virtual ViewX. The user account is required to run the ViewX processes that are created on that server machine. It is important that this user account is not deleted, nor its password changed, otherwise Virtual ViewX will be unable to operate.
The automatically created user account is assigned the  name VVXLocalUser.
Do not confuse this user account with the 'configured' Geo SCADA Expert User Accounts that are required to enable users to access the Geo SCADA Expert database from Virtual ViewX clients (see Overview of User Account Security).
Further Information