Configure a Wonderware Historian Database Item

To configure a database item that represents a connection to a Wonderware Historian, you need to display the Wonderware Historian Form (see Display a Form) and configure the relevant settings on that Form.

The Form has several tabs:

Use the fields on the Wonderware Historian tab to define the connection properties that enable Geo SCADA Expert to communicate with the Wonderware Historian server:

For information about configuring properties in the Tag Names, Connection, and Store/Forward sections of the Wonderware Historian tab, see the relevant topics in this section. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Specify the points and/or accumulators for which you want to export historic data using the Wonderware Historian database item: see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2021