MinEU

Description

The minimum value of the tag, measured in engineering units.

Geo SCADA Expert Metadata Field

WH_MinEU

Default Value

This is the minimum value configured for the point's engineering range (if it has a range). For analog points, the range is zero scale to full scale. Therefore, the default minimum value is the zero scale. For digital points and counter points, the default minimum value is 0. Other types of point, such as rate of change points, have no minimum value and therefore use the Wonderware Historian default (which is 0). Some other types of point (such as minimum, maximum and mean points) use their parent point for the default minimum value.

Type

Double.

Further Information

MaxEU


Disclaimer

Geo SCADA Expert 2021