Connection Alarm

Associated with: Wonderware eDNA Historian database item.

The Connection Alarm attribute indicates the status of a network connection between the eDNALinkMx API and a Wonderware eDNA Historian server.

The connection status can be as follows:

For more about the primary and secondary connections, see Specify the Connection Properties

The Geo SCADA Expert alarm message includes any error message generated by eDNALinkMx.

Possible States: Displays one of the Geo SCADA Expert Standard Alarm States.


Disclaimer

Geo SCADA Expert 2021