Secondary Connection State

Associated with: Wonderware eDNA Historian database item.

The Secondary Connection State attribute indicates the status of the secondary network connection between eDNALinkMx and the Wonderware eDNA Historian server.

For more about the primary and secondary connections, see Specify the Connection Properties

The possible connection states are:

Further Information

Specify the Connection Properties


Disclaimer

Geo SCADA Expert 2021