Configure the Fonts used for the Axis and Trace Labels

You can change the appearance of the font that is used for the x-axis text. You can also change the appearance of the font that is used for the trace labels. You do this using fields in the X-Axis Properties window (see Configure the X-Axis Properties).

Use the Fonts section of the window to specify the font's appearance:


Disclaimer

Geo SCADA Expert 2021