Remove a Trace

To remove an obsolete trace from an X-Y-Z Plot:

  1. Display the X-Y-Z Plot in Design mode (see Display an X-Y-Z Plot in Design Mode).
  2. Right-click on the tick (short line) that indicates the trace's position on the x-axis.
    A context-sensitive menu is displayed.
  3. Select the Remove Trace option.
    The trace is removed from the X-Y-Z Plot.
  4. Select the Save button to store the change to the X-Y-Z Plot.

To temporarily hide the set of information that is associated with an individual trace: see Show or Hide the Whole Trace Entry.


Disclaimer

Geo SCADA Expert 2021