Reset the Zoom Level
            You can Zoom In or Out and Pan Along the X-Axis on an X-Y-Z Plot. To return the x-axis to show its full span, you reset its zoom level. To do this:
- Right-click on the x-axis.
A context-sensitive menu is displayed. - Select the Zoom option.
A further context-sensitive menu is displayed. - Select the Reset Zoom option.
The x-axis zoom level reverts back to show the full range that is defined for that axis.