Using X-Y-Z Plots

You can use X-Y-Z Plots to view the relationships between multiple sets of historic values on a single graphical display. Each X-Y-Z Plot is configured to provide specific data over a specified time period. By accessing an X-Y-Z Plot in Run mode, you can view the data on the plot, alter the appearance of the X-Y-Z Plot, and show or hide information associated with individual sets of historic values.

If you are unfamiliar with X-Y-Z Plots, we suggest that you first familiarize yourself with their layout (see Understand X-Y-Z Plots).

The following topics explain how to access an X-Y-Z Plot in Run mode, use its navigation features, alter the plot's appearance, and show or hide various features. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021