Monitoring the State of PSTN Communications on your System
You can use Status displays to check on the status of individual channels or outstations (see Status Displays), and
- Channel Scanning Statistics List
(this includes the number of messages that have been sent to the outstations via each channel, and how many of these messages succeeded or failed, since the statistics were last reset) - Channel Serial Port Statistics List
- Outstation Comms. Statistics List
- PSTN Channel Calls List
- PSTN Outstation Calls List.
The Lists are available from the Queries Bar.