Specify the Network-Connected Channels on Which the Driver Accepts Inbound Connections

This section applies to shared outstations:

Use the Inbound Connection combo box to specify on which line(s) Geo SCADA Expert is to accept inbound network connections. (An inbound connection is attempted whenever the outstation tries to instigate communications with Geo SCADA Expert, rather than vice versa.)


Choose from:

Accept Inbound Connections on Both Lines

Geo SCADA Expert will accept inbound connections on either of the network-connected channels on which the outstation can communicate.

If the inbound connection occurs on the channel that is not currently assigned to the outstation, the driver will automatically switch the outstation (and any Group Slave outstations for which that outstation is Group Master) to the other channel (the one on which the inbound connection occurred). If heartbeat polling is used, this will also change channels, so that the server continues to send ‘heartbeats’ via the channel that is not being used by the outstation.

Only Accept Inbound Connections on Current Line

Geo SCADA Expert will only accept inbound connections on the network-connected channel that is currently assigned to the outstation.

Any attempt to connect to Geo SCADA Expert via the channel that is not currently in use will be rejected.

With an Independent shared outstation, if the Geo SCADA Expert Server Configuration Tool’s option to ‘Allow channels on a driver to share the same listen port’ is enabled:

(If the ‘Allow channels on a driver to share the same listen port’ option is disabled, any attempt to connect via a channel other than one that is assigned to the outstation set will be rejected. Geo SCADA Expert will only accept inbound connections on the channel that is currently assigned to the outstation (unless the outstation is configured to Accept Inbound Connections on Both Lines).)

With an outstation that has a Switch Type other than ‘Independent’:

For information on the ‘Allow channels on a driver to share the same listen port’ option, see Define whether a Listen Port can be Shared.


Disclaimer

Geo SCADA Expert 2022