Configure the General Time Point Properties

On the Advanced Modbus driver, Generic Time Points are currently only supported for use on the Lufkin SAMS driver. That driver is an extension of the Advanced Modbus driver.

Use the fields at the top of the Time Point tab on the Advanced Modbus Time Point Form to Configure Common Point Properties. Fields that are specific to Advanced Modbus Time points are explained below.


Disclaimer

Geo SCADA Expert 2022