Introduction to the Advanced Modbus Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Advanced Modbus items and features in the Geo SCADA Expert database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s Advanced Modbus driver. The Advanced Modbus driver enables Geo SCADA Expert to communicate with Modbus controllers using the Modbus protocol suite.

The Advanced Modbus driver provides functionality that enables Geo SCADA Expert to communicate with Modbus® controllers, using the Modbus® protocol suite (see Which Driver?). The Modbus communication types that the driver supports include:

Geo SCADA Expert can communicate with Modbus controllers directly, using direct or PSTN communications. Function codes supported by the Advanced Modbus driver determine how it reads or writes to data on the controllers (see Modbus Function Codes Supported by the Geo SCADA Expert Advanced Modbus Driver).

Geo SCADA Expert can also provide a communications ‘gateway’ to allow applications such as ISaGRAF®, to communicate with Modbus controllers remotely, via the same communications link (for example, in situations where a controller has only one radio link). With the latter set-up, a Remote Connection database item provides a TCP/IP socket connection between Geo SCADA Expert and the remote application.

The Advanced Modbus driver documentation:

The documentation also explains:

Some controllers with which Geo SCADA Expert can communicate using the Advanced Modbus driver, support additional features that do not apply to other Modbus controllers. Where Geo SCADA Expert uses an Advanced Modbus Extension Driver to support such features, use the guide to that extension driver in conjunction with this guide.


Disclaimer

Geo SCADA Expert 2022