Specify the Point Address Range

Use the Point Address Range field on the '<Driver Type>' tab to specify whether the points on a controller use a 5 Digit or 6 Digit address range. Geo SCADA Expert performs configuration time-range checking on the controller’s points according to this property.

Specify whichever address range is supported by the controller. If your system is running an Advanced Modbus extension driver, check whether the relevant extension driver guide provides more information about the Point Address Range that is supported.

Specify the actual point addresses on the individual Point Forms (see Configure Common Point Properties).


Disclaimer

Geo SCADA Expert 2022