Specify the Set Address

Geo SCADA Expert uses a Set Address to identify each Modbus controller that dials in to the system, or uses a remote connection to communicate with Geo SCADA Expert. The Set Address defines the group to which each controller belongs. The address is used internally by Geo SCADA Expert—it does not exist in the controller hardware.

Use the Set Address field on the Modbus tab to specify the address of the set:

Geo SCADA Expert automatically allocates the next available address to a set, whenever a set is created in the database. The allocated address is displayed when you open the Form.

If you want to specify a particular address, overwrite the entry in the Set Address field.


Disclaimer

Geo SCADA Expert 2022