Disable Group

Associated with: Advanced OPC Groups

Security permission required to access this pick action: Disable Group

Use the Disable Group pick action to take an Advanced OPC Group Out of Service, so that the Group is no longer active.

Be aware that disabling a group de-activates all the items associated with the group, although their configuration will remain unchanged.

Use the Enable Group pick action to place the group back In Service. An entry is logged in the Event Journal whenever either pick action is used. The message indicates whether the group has been enabled or disabled.

NOTE: The 'Disable...' series of pick actions are assigned the 'Disable Points' security permission so that users with that permission can disable database items without necessarily being given the full 'Configuration' security permission. A user, such as an operator, whose User Account is given the 'Disable Points' permission but not the 'Configure' permission can disable a database item, but is prevented from altering the rest of that item's configuration.

NOTE: If using this pick action with the Automation Interface, you have to specify the method name Disable.


Disclaimer

Geo SCADA Expert 2022