Disable Switching
Associated with: Advanced OPC Groups
Security permission required to access this pick action: Switch Line
Use the Disable Switching pick action to stop an OPC Group from being switched to other OPC Servers within a multi-server configuration.
Use the Enable Switching pick action to re-enable switching between servers.
ATTENTION: If switching is disabled, then automatic switching, when a server fails or a group associated with a server fails, is blocked and the Switch Server pick action is disabled.
NOTE: If using this pick action with the Automation Interface, you have to specify the method name EnableSwitching.