Understand Alarm Redirection

If required on your system, you can configure Geo SCADA Expert to redirect alarms for:

For each of the above, you can configure up to 15 alarm redirections, each of which can be configured to trigger automatically, manually, or both. In each case, you configure the alarm redirections on the Redirection tab of the appropriate configuration Form. You specify the alarm redirections in the order in which Geo SCADA Expert is to check them: from the top row downwards. For each alarm redirection that is required, you specify the conditions under which Geo SCADA Expert is to redirect the alarm, the action that is to be performed, or the Action Roster or redirection Calendar that is to come into force.

When an alarm occurs, Geo SCADA Expert checks the trigger type of the action, action roster, or alarm redirection calendar at the top of the Redirection tab downwards, on the affected system, Group, or individual item.

For each alarm redirection that is to trigger automatically:

For each alarm redirection that is to be triggered manually:

For each alarm redirection that can be triggered both manually and automatically:


Disclaimer

Geo SCADA Expert 2022