Confirm that the Required Geo SCADA Expert Components are Installed
Before you can use Aquis with Geo SCADA Expert you need to confirm that the Aquis components of Geo SCADA Expert are installed on the Geo SCADA Expert clients and servers.
On each Geo SCADA Expert client and server on your system, use the Change function of the Programs and Features item in the Windows® Control Panel to see if the required Geo SCADA Expert components are installed.
The required components are:
- ViewX Aquis Client - on all Geo SCADA ExpertClients
- Geo SCADA Expert Server Aquis Database Module - on all Geo SCADA ExpertServers.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.