Displaying System Time Series

To display a pre-configured time series for the whole system. Each time series can show anything from one attribute for one object to many attribute of a number of objects:

  1. Right-click within the Main view area.
    A context-sensitive menu is displayed.
  2. Select the Time Series option.
    Another context-sensitive menu, listing all the available Time Series is displayed
  3. Select the time series you require.
    A Time series window is displayed, the example illustrated shows a Main Balance graph for the whole system
  4. Close the window to return to the Main view area.

Further Information

Printing


Disclaimer

Geo SCADA Expert 2022