CFX Specific Alarm and Event Categories

Each alarm and event on a Geo SCADA Expert system has a Category that indicates the type of alarm or event. The Category is included by default in the Events List and, if applicable, the Alarms List and the Alarm Banner.

You can optionally filter the entries in either List by category—the entries from which you can choose comprise various ‘core’ categories, along with any categories that are specific to the drivers that are installed on your system.

On systems on which the CFX Export driver is installed, in addition to the ‘core’ alarm and event categories, this CFX-specific category is available:

Further Information

Events Lists and ‘core’ filter categories: see the Geo SCADA Expert Guide to Lists.

Alarms Lists and ‘core’ filter categories: see the Geo SCADA Expert Guide to Alarms.


Disclaimer

Geo SCADA Expert 2022