Change the Port for the Server’s Incoming Data

By default, each Geo SCADA Expert serveruses Port 5481 to receive data from a client via the client - system connection. For many systems, this default setting is suitable. However, if Port 5481 on your server is unavailable, you will need to change the port setting so that Geo SCADA Expert uses a different port for client to server communications.

To change the port used by the server to receive data from a client:

  1. Display the Server Configuration Tool and log on if required.
  2. Expand the Global Parameters branch.
  3. Select the Advanced entry.
    The Advanced settings are displayed.
  4. In the Server Port field, enter the number of the port that is going to be used instead of Port 5481. You have to enter a valid and available port number.
  5. Define the other settings for the server port if required (see Connection and Update Settings in the Geo SCADA Expert Guide to Server Administration).
  6. Apply the changes to the server.
    The new server port settings are put into effect.

ATTENTION: Remember that if you are using a firewall, you will need to reconfigure it so that it allows the newly defined server port to receive and send data via the client - system connection.


Disclaimer

Geo SCADA Expert 2022