Define How a Boolean Value is Displayed
Select the Boolean category in the Text Format window to use a format that is the Boolean (True or False) equivalent of a numeric value. For instance, if you want to display the value of a 1-bit digital point (0 or 1) as the text ‘F’ or ‘T’.
Any non-zero numeric value is treated as a Boolean ‘True’.
Select the required format from the list in the Type field.
The example in the Sample area updates to show how the value will appear