Edit a Data Set Existing Field

To edit an existing field on a Data Set:

  1. Display the Data Set in Design mode (see Edit a Data Set).
  2. Double-click on the Data Set in the Database Bar.
    The Data Set is displayed in Design mode with existing fields displayed.

  3. Right-click on the field.
    A context sensitive menu is displayed.
  4. Select the Properties option.
    The Edit Field window is displayed.

  5. Use the window to Specify the Data Set Field Properties.

Disclaimer

Geo SCADA Expert 2022