Edit an Existing Field
To edit a field on a Data Table:
- Display the Data Table in Design mode (see Edit a Data Table).
- Right-click on the field.
A context sensitive menu is displayed. - Select the Properties option.
The Edit Field window is displayed. - Use the window to Specify the Field Properties.