Interval

Associated with: Master Station Accumulators on which the total is reset on an End of Period basis

This status attribute indicates the interval at which the Accumulator’ is configured to reset. The interval is specified using the Interval field within the End of Period Reset section of the Accumulator Form (see Specify the Period over which an Accumulator’s Value is Calculated).

Use the attribute in conjunction with the Start of Interval and End of Interval status attributes.


Disclaimer

Geo SCADA Expert 2022