Produce a Profile Based on Historic Data
You can produce a Time Profile that is based on actual data by temporarily importing historic data into the Time Profile window. You can then use the data to produce a profile:
- Automatically, by getting Geo SCADA Expert to insert vectors based on that data (see Use Gaussian Distribution Calculations to Produce a Profile from Historic Data).
- Manually, by adding the vectors yourself, to produce a profile based on the historic data (see Manually Produce a Profile Based on Historic Data).
As an alternative to the above, you can write a program to Generate a Profile’s Data Programmatically.