Specify an Accumulator’s Source

Use the fields within the Source Object section of the Reset tab to specify the item that is to provide the source for an Accumulator and the type(s) of data that the Accumulator is to process from that source:

If the source of an Accumulator is a point, you might well have to select more than one of the above check boxes in order for the Accumulator to process the required data. For example, you might select both 'Current' and 'Value Change' when the source is an analog point, or 'Current' and 'State Change' when the source is a digital point. Additionally, if End of Period or Timed Reporting ('background logging') is supported by, and configured for, the point, you might also select the check box(es) that relate to that type of logging.

The reasons for logging vary, depending on the type of driver and point, the features they support, their configuration, and so on. The Historic List for a source point has a 'Reason' column, which indicates the reason why Geo SCADA Expert has stored each point value historically. You might find this information useful when setting up an Accumulator (see Understand Historic Lists in the Geo SCADA Expert Guide to Lists).


Disclaimer

Geo SCADA Expert 2022