Specify the Properties Associated with Corrupt Record Alarms

The configuration Form of the Root Group includes Alarm Summary, Configuration Changes, Historian, and Event Journal tabs. Each of the tabs include a Corrupt Record section that allows you to define the severity of alarms generated when corrupt historic records are encountered. In addition you can limit the maximum number of alarms displayed by Geo SCADA Expert.

Use the following fields to define the severity and maximum number of alarms displayed:

Further Information

Alarm Categories.

Use the Server Status Tool to assess the Corrupt Count and Corrupt File status of invalid historic records: see Historian.


Disclaimer

Geo SCADA Expert 2022