Text String Syntax
The syntax for text strings is given below:
Code | Description |
---|---|
> |
Forces the whole string to appear in upper case |
< |
Forces the whole string to appear in lower case |
Example:
The syntax > is used to force the incoming string value ‘Xerox 123’ to be displayed within Geo SCADA Expert as ‘XEROX 123’.
The syntax < is used to force the incoming string value ‘Printer TRAY 5’ to be displayed within Geo SCADA Expert as ‘printer tray 5’.