Trend - Annotation
Associated with: Trends
The Annotation state is indicated by a light-blue marker (by default) on a Trend’s trace.
The color indicates that an annotated comment exists for that entry on the trace. The annotation might, for example, explain the reason for a particular value appearing on the trace (see Trend Annotations).
Place the cursor over the indicator to display a ToolTip showing the annotation, or view the annotation using an option on the context sensitive menu.
For data sources that exist in the Geo SCADA Expert database, Geo SCADA Expert obtains the marker color from the data source's Color Palette. The exception to this is if Geo SCADA Expert is unable to obtain the marker color from the server (for example, if communications with the server is interrupted when a Trend is redrawn). In such a situation, Geo SCADA Expert uses the marker color that is specified in the Options window. Geo SCADA Expert also uses the marker color from the Options window for data sources that are from a non-Geo SCADA Expert database (for example, another OPC database).