Quality
Associated with: Crystal Reports
This attribute indicates the quality of a report’s data.
Possible States:
- Good—The report has valid configuration.
- Out of Service—The report is not functional (online) as it is configured as not In Service. Check with a system administrator as to whether the report should be put online.
- Not Connected—The report has no definition (it is a new, blank, report). An engineer needs to specify the required report content and layout using the Crystal Reports application (see Configuring the Report Structure and Basic Content).
- Configuration Error—Part of the report’s configuration is invalid. Correct the configuration errors. (For more information, see Checking for Invalid Configuration in the Geo SCADA Expert Guide to Core Configuration).