DNP3

Configure Alarm Limits

Use the fields within the Alarm Limits section of the Counter Point or Frozen Counter tab to set the limit values for the point and specify whether an alarm or event is generated if the value of the counter rises to, or exceeds, a limit.

For information on configuring a counter point’s High High and High limits, and the properties for when the counter is in its Normal operating range, see Configure the Limits for a Counter-Type Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the Tune Limits property, see Define Whether a Counter-Type Point’s Limits can be Tuned in the Geo SCADA Expert Guide to Core Point Configuration.

If the Area of Interest feature is enabled on your system, an Area of Interest field is displayed within the Alarm Limits section. For information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2022